This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about most up to date CCS and software components to install for DSP/BIOS and C55xx devices ?

Hi,

In a previous post it was mentioned that the most up-to-date offering for support for DSP/BIOS based projects on the TMS320C55xx devices is the following :

DSP/BIOS 5.42.00.07 and DSP/BIOS 5.42.02.10
CCS 7.3 or later
CGT for C5500 4.4.1
XDCTools 3.24.05.48
XDAIS 7.24.00.04

Can I get a confirmation please that this is indeed correct as I do not see any mention for these devices in the release notes for the XDCtools 3.24.05.48 whereas previous version of XDCtools were explicitly mentioning support for the C55 devices....

Device Support

This release supports the following device families:

    C6000 family - C674, C67P, C64P, C66, C64T
    C2000 family - C28
    ARM processors - TMS470, ARM7/9, Cortex A8/M3/R4
    MSP430
    Native development host (Windows, Linux)
C55 ?????????????

So otherwise if this was an oversight, what would be a more suitable CCS version XDCtools version etc that would work with DSP/BIOS based projects and projects ported from CCS 3.3 for instance ?

Thanks in advance and regards,

citizen