In "[: too many arguments" error from loadti.sh in CCS 10.3.0 under Linux was attempting to post some text into the code editor to get the formatting correct.
However, attempting to paste that text into the code editor resulted in the following error:
So, I had to paste the text into the post without using the code editor.
I can paste other text into the code editor without error, so maybe the text contents is confusing some parsing. The error was repeated with Opera and Firefox web browsers under Linux.
The problematic text is attached as a file if someone wants to repeat the issue. The language in the code editor was set to "text", but got the same error when tried other languages.
$ ~/ti/ccs1030/ccs/ccs_base/scripting/examples/loai/loadti.sh -c ~/E2E_example_projects/TMS570LC4357_GCC_halcogen/targetConfigs/TMS570LC43xx.ccxml ~/E2E_example_projects/TMS570LC4357_GCC_halcogen/Debug/TMS570LC4357_GCC_halcogen.out /home/mr_halfword/ti/ccs1030/ccs/ccs_base/scripting/examples/loadti/../../bin/dss.sh: line 52: [: too many arguments ***** DSS Generic Loader ***** START: 10:12:47 GMT+0100 (BST) Configuring Debug Server for specified target... Done TARGET: Texas Instruments XDS110 USB Debug Probe Connecting to target... CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 testEnv.outFiles: /home/mr_halfword/E2E_example_projects/TMS570LC4357_GCC_halcogen/Debug/TMS570LC4357_GCC_halcogen.out Loading /home/mr_halfword/E2E_example_projects/TMS570LC4357_GCC_halcogen/Debug/TMS570LC4357_GCC_halcogen.out CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset Done Target running... Interrupt to abort . . .