This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IBIS models

Prodigy 160 points

Replies: 4

Views: 693

Hi,

 

I need IBIS Files for the following chip, kindly share quickly.

 

  1. TPD2EUSB3.0 - SOT23-3 ESD PROT IC
  2. TPS2115ADRB - SON-8
  3. TPS2553DBVT - SOT23
  4. TPS650061RUKT - QFN20

Thanks,

Gang

4 Replies

  • Moving to the appropriate forum.

  • Hi Gang,

    I'll submit a request to model the TPS devices. If you are requesting IBIS models, then you know that the only buffers suitable are digital. On these devices, those are the EN inputs and Open-drain status outputs.

    For the TPD2EUSB3.0, there is a model already for the TPD2EUSB30A that you can use.

    Regards,

    David Larkin

    Webench Design Center

  • In reply to David Larkin - WEBENCH Design Center:

    Hi David,

    Thanks for the reply.

    Please share the IBIS models for TPS devices quickly.

    For TPD device, i'll take the TPD2EUSB30A device data.

    Regards,

    Gang

  • In reply to gangu.C:

    Gang,

    You can use the IBIS model for the TPS2553-1.

    David

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.