This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDA-01237: TIC12400-Q1

Prodigy 185 points

Replies: 1

Views: 396

Part Number: TIDA-01237

Hello TI team,

I wondering if the CCS software files

are available for the reference design

used with the MSP430 Launchpad.

Thank you!

  • Hi Moises,

    The TIDA-01237 was not intended to be a orderable design so the software I developed for it did not go through the TI software release process and therefore is not ready to be shared publically.

    We do however have an EVM and a GUI for evaluating the device. In the GUI all the device inputs and settings can be manipulated and then the GUI will generate the list of SPI commands that need to be sent to the TIC12400-Q1 device for evaluation.

    www.ti.com/.../TIC12400EVM-KIT

    The GUI is available for free without needing to get the hardware and you can set up thresholds, interrupts, wake up settings, etc, and then you can go to the register tab in the GUI to see what values need to be written to all of the registers. I used this when evaluating the design.

    Please let me know if you have any other questions,

    John

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.