This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDA-00281: Software control for BLDC motor

Intellectual 380 points

Replies: 5

Views: 179

Part Number: TIDA-00281

Hello,

I am looking for a reference software for the design TIDA-00281, I have found tidcbd2 file, which includes some files from the motorware at path:

E:\sw\modules\hal\boards\TIDA-00281\f28x\f2802x\src, as per path it can be observed that it related to motorware path, but inside the

path:C:\ti\motorware\motorware_1_01_00_18\sw\modules\hal\boards, there is no such folder name as a TIDA-00281.

  • Hello, did you download the software package from ti TIDa-00281 product page?

    Regards, Jiri

  • In reply to Jiri Panacek85:

    Yes, it includes various code, lab01, lab02, etc, but I didn't found the files.

  • In reply to kishan pala:

    Follow the directions in section 6 of the reference manual.  You have to first install Motorware, then add the TIDA-00281 files from the zip into the correct subdirectories, as discussed in section 6.2 of the manual.  This will then include the user.h file and the hal files in the correct locations.

    -- Clark Kinnaird

  • In reply to Clark Kinnaird:

    Thank you Jiri and Clark, I have followed the instruction from section 6.2, but still have same problem, I have attached the screenshot for the reference.

  • In reply to kishan pala:

    Here is what my project structure looks like:

    -- Clark Kinnaird

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.