Is the attached design based on TPS40303+TPS54418,can be simulate with TINA ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I suppose that depends on what parameters or operating conditions you want ot simulate...
Eli,
There are TINA reference designs available for the TPS40303 and TPS54418 in TINA that could be modified to simulate the blocks that are shown in the pdf file you attached. I am not exactly sure what you are asking. The models have been verified on the reference designs for correct operation. I believe that these blocks could be simulated with the TINA models that are currently on the Web.
Please remember that there are other parts in the pdf file as well that may need to be used in conjunction with the TI models. I cannot give you any information on the use or accuracy of those models.
I would pull down the reference design for the TPS40303 (or the TPS54418) from the prodcut folder, modify it to the block in the pdf and run the simulation. Please note that the simulation may take longer to run than the existing reference design.
Britt