Other Parts Discussed in Thread: TINA-TI
I performed Fourier series for my schematic and got about 0.036% THD. Base frequency 10khz, start time is 10msec, end time in transient analysis is 100msec. It was strange and I reconnected "out" port directly to Voltage Generator. The result was 0.035% again! I checked internal impedance of VG1 - it was 0 ohms. I disconnected VG1 from my amplifier and did the test again. The result is 0.000000...% - it is expected result with ideal sinus source with Ri=0.
Questions:
1. Why I don't see zero THD on output of ideal sinus generator with internal impedance 0 ohms when I connect it to my circuit with non-zero input impedance?
2. Why the amplitude of first harmonic is not correct and doesn't follow the amplitude parameter of Voltage Generator?