Hello,
I am designing a +/-12VDC supply based on LM25575 converters used in cascade. The topology consists to create a +12V from 24VDC (coming from PLC backplane). From the +12V we create the -12V by using the LM25575 converter in inverter mode.
The topology and peripherical components comes from the results of the WEBENCH designer tool. However, when I want to simulate the circuit, the -12V polarity doesn't work.
So, I would like to know if the problem comes from the topology or is it a limitation of the model ?