Hi,
I had a design went through below for a 24V to 5V@15A buck a few days back.
Design : 4561043/188 LM5116MHX/NOPB
LM5116MHX/NOPB 22.0V-26.0V to 5.00V @ 15.0A
Now I ran the same settings with webench and only 4-5 options to choose. This design is no longer there due to no FET to select. Actually what I am trying to do is to replace the Infineon FETs with CSD18504Q5A and CSD18537NQ5A to see if they works better in webench simulations.
If you can't pull the old design I can attach pdf here.
Any help or comments are appreciated.