Hi Support,
how do we suggest to test 2.5 - 10 PPM identification with our TIDA-00378? Wich kind of tools can customers use to characterize this?
Thanks and regards,
Alberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support,
how do we suggest to test 2.5 - 10 PPM identification with our TIDA-00378? Wich kind of tools can customers use to characterize this?
Thanks and regards,
Alberto
Hello Sean,
While I'm doing some additional research on this, I'm wondering if you read in detail the setup and testing guide provided: www.ti.com/lit/ug/tidub65c/tidub65c.pdf ?
~Leonard
Hi Alberto,
The design guide describes the equipment we used to characterize the design. For quick lab tests I would suggest the DUSTTRAK DRX AEROSOL MONITOR 8533. These can be rented (or purchased) and have good accuracy. The only thing about these is that they measure particle mass, not particle count. Also, you still need a mechanism to generate particles (dust, smoke, etc.).
For a full characterization test, you probably want to use a 3rd party lab. Intertek in the NY area has a lab set up for air purifiers which can be re-purposed for particle sensor tests.
Gus
Hi Sean,
The airflow we used for our tests is documented in the design guide. That was dictated by the airflow of the equipment we used to characterize the design. Unfortunately, we didn't do testing using different airflows to understand impact on accuracy.
Gus Martinez