This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00322: TIDA-00322

Part Number: TIDA-00322
Other Parts Discussed in Thread: UNIFLASH, TDC1000

Hello,

I have designed a custom board based on the TIDA-00322 reference design. I have used the same parts you provided in the schematic. I also succeeded in programming the MCU via JTAG with the help of the XDS100V2 debug probe. I uploaded the TDC1000_C2000_FW-v1.42-1MHz.hex file from the TEXAS INSTRUMENT\FIrmware folder using UNIFLASH as flashing tool. Is this the right hex file or do i need to upload a different one?  Also, will the GUI you provided work with my board? I'm asking this because when i open the GUI in the select port section my board appears on COM3 but when i hit the connect button however it says "Connect failed! Check the COM port number". I am running windows 7.

Thanks, 

Florin