Part Number: TIDA-00067
Champs,
I am asking this for customers.
They are looking for
1) PLC on 48 V DC, but the DC will be changing 40V to 60V
2) Bit rate is larger than 250 kbps
3) Transmission distance is about 1 meter
4) Support CAN input or CAN output. That is, CAN to PLC or PLC to CAN
Do you think this TIDA-00067 can be leveraged for above four or at least the first three requirements?
Or do you have any other suggestion?
Wayne