Other Parts Discussed in Thread: TPS61021A
Tool/software: WEBENCH® Design Tools
Hello
I have a questions regarding TIDA-01385 refference design for energy harvesting. I'm currently working on energy harvester project. The energy that will be harvested is magnetic field from power line, with the current flows is about 100 A to 400 A. I will use the CT as energy harvester, and TIDA-01385 as circuit to harvest the energy. The CT that will be used has ratio primery to secondary at 100 : 0.05A. The system purpose is to detect the power consumtion and send the data using LORA wireless communications . I will use ESP-WROOM 32 as MCU, ATM90E26 as current sensor, and Rak811 as transceiver dvice. The maximum current consumption for all those device is about 200ma at 3.3 V. My question is, is the TIDA-01385 wll meets my power consumption needs?. it is about 660mW.
Thank you and Best Regards.