This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00779: tida-00779

Part Number: TIDA-00779
Other Parts Discussed in Thread: TIDA-00443

looking to boost follower control circuit in tida-00779 Emitter resistor of Q4(R14) is 13.7K and bottom feedback resistor (R9) is 13K. as per TIDA-00443 it is mentioned that ratio between Emitter resistor and bottom feedback resistor should be 1:2 then why 1:1 ratio is maintained Between those resistors in  TIDA-00779 and in TIDA-00443. Because if feedback resistors  selected as per boost follower circuit calculations output  of pfc stage get reduced by great extent.