Part Number: TIDA-01622
Could you provide me the spec of the transformer ,and tell me the switch freqency of every MOSFET in the system
and the product have any sample i can buy?i'am a student from Tiawan thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01622
Could you provide me the spec of the transformer ,and tell me the switch freqency of every MOSFET in the system
and the product have any sample i can buy?i'am a student from Tiawan thank you
Hi,
The transformer spec:
Winding spec: Np:Ns:Naux1:Naux2=22:4:5:13;
Core spec: RM8 size/3F36 material;
For Active clamp Fly-back, the switching frequency varies with input voltage and output current.
For this design, the maximum switching frequency is about 400Khz.
Which sample do you refer? If for ACF controller, SR driver, or isolator, you can request the sample through ti.com.
If for Transformer, I can share with you that the part number is 750343803, you can request it from Wurth.
If for GaN-FET in this design used, because it is from Navitas, you can contact the Navitas company.
Thanks very much!
BR
Liu Cheng