Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hello everybody,
I have a question regarding the possibilities to flash the TIDA-00489. From the PDF document http://www.ti.com/lit/ug/tiduau1b/tiduau1b.pdf I can see, that there is a JTAG programming interface.
- Is there a convient way to connect this board to a USB port of a computer? Something like the SmartRF06 Eval Board but cheaper...
My second question is regarding Over-the-Air Download (OAD) to quickly update many sensors in a network. So I was thinking, there are 10 sensors and 1 collector which is connected over a gateway to the internet.
- Is it possible to update the TIDA Software on the sensors "from home" over the internet?
- Or is it at least possible to update the sensors with a laptop when I am nearby without connecting via JTAG?
Hope you guys can help me out again.
Kind regards
Stefan