This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00909: TIDA-00909

Part Number: TIDA-00909
Other Parts Discussed in Thread: TIDA-00913

Hello there,

The "user_j5.h" header file is missing from tida 00909 software package? Is it possible to use the "user_j5.h" found on in tida 00913 software package?

Regards,

AB

  • Hello Abdallah Alansaari,

    thank you for pointing out the missing header file "user_j5.h" in the TIDA-00909 software files.

    Yes, as you indicated you can definitely use the "user_j5.h" from TIDA-00913 software files. It is the same settings, the only difference between the two files is that instead of TIDA-00909 the comment lines it refer to TIDA-00913. Therefore it does not impact the compiler, however you may want to change though. I apologize for the inconvenience.

    We will update the TIDA-00909 software package as soon as possible.

    Regards, Martin