This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIDA-01469: CCS/TIDA-01469

Prodigy 30 points

Replies: 1

Views: 277

Part Number: TIDA-01469

Hi,

This is Sarath Kumar from India. I have two questions to ask here.

Question 1:

We are trying to use TIDA-01469 from TI with other microcontrollers. Does TI have any support for using TIDA-01469 with any other microcontroller apart from TI controllers?

Question 2:

Where can we find support for tuning CC1350 sub-1-GHz to 865-867 MHz, because in India licence free band starts from 865-867 MHz? If we can tune CC1350 to 865-867 MHz it will be great, then we will use TIDA-01469 with CC1350 itself.

  • Hi Sarath,

    SarathKumar C
    We are trying to use TIDA-01469 from TI with other microcontrollers. Does TI have any support for using TIDA-01469 with any other microcontroller apart from TI controllers?

    We don't have the code available for any other microcontroller, unfortunately.  Your best bet would be to take an example project from the microcontroller you want to use and port over the code portions you need from TIDA-01469, e.g. FFT routine.  I recommend you check the TI resource explorer for example code (http://dev.ti.com/tirex/#/).

    SarathKumar C
    Where can we find support for tuning CC1350 sub-1-GHz to 865-867 MHz, because in India licence free band starts from 865-867 MHz? If we can tune CC1350 to 865-867 MHz it will be great, then we will use TIDA-01469 with CC1350 itself.

    TIDA-01469 uses Bluetooth, so it runs in the 2.4GHz band.  You can check the TI resource explorer for example code that use the CC1350 in the Sub-1GHz band.  You would need to port over the applicable code portions from TIDA-01469.

    I hope this helps!

    Gus Martinez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.