Part Number: TIDA-01627
HI there,
I have two questions about the TIDA-1627.
Firstly, can you set the 65987D as default-source? I do not want to have mechanic parts in my design and do not want to include a button, also I dont see a need for it. If it acts as default-source, then it will charge anything that is plugged to it (which is the point of a power bank) and will only sink when connected to a wall charger. Perfect!
How can I include this into the code?
Also, since this is my very first USB-C Device, is there any code to start working with such as the code used for the reference design?
Thank you very much,
Karim