Part Number: TPS7A33
Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello,
I have built an LTSpice model (shown in the attached) for the TPS7A4700 and TPS7A33. When I add resistors, it still functions. Likewise the Balanced Line Receiver THAT 1200 works well too, when using voltage supplies provided in LTSpice. However, when I add the THAT 1200 Balanced line receiver, the circuit no long works. It appears to start out with a DC voltage on the output, which I think may be affecting the output regulation function.
Can you please have a look and see if you see any clues as to why this would happen?
Thanks in advance,
Cody