Part Number: PMP20289
Hi
We are trying to bulid a 500 W Half Bridge LLC using LMG3410. we gone thro the PMP20289 reference design. KIndly clarify on the below.
1. For the given spec, the value of resonant tank components is coming around Lr= 7.8 uH and Cr=26 nf. pls clarify what is the actual value of
Lr and Cr used ? In the schematic it shows 6 nos 8.2 nf connected in parallel (C111 to C116) is all these capacitors populated in the board ?
2. In the schematic, between the main planar tranasformer primary and the resonant capacitor, another transformer is connected in series , i guess
for current sensing, which has a inductance of 40 mH. How could we connect such an high inductance value in series with the resonant tank ? kindly clarify ..
3.what is the value of output capacitor used ? In the schematic i was able to see 2 x 1 uf and a 0.1 uf cap..
The schematic i referred is PMP20289 Schematic and Block Diagram.
Kindly clarify on the above.
Thanks
Lenin.