While turning on the PFC output DC voltage was 389 V.
Then increased load up to 3.6KW in steps of 240W and voltage was stable at 389 volts.
Then I kept it running as it is for a long time. As the time proceeds the output DC voltage seems to be slowly rising.
so I run it for a very long duration of time.
in 2-3 hours voltage raised up to 401 volts. then in the next 4 hours, it raised up to 403V only and seems to be stable at 403 volts.
Is it a desirable condition?
What can be the possible reason for this?
Thanks.