I'm not sure if this is the right place to post this, but there appear to be a number of errors in the DP83825I Ethernet Phy datasheet. Not unexpected for something so new.
I think the value labeled T2 in Fig 5 should be labeled T4.
based on the text:
The text of bit 5 in table 8 appears to be wrong:
I apologize if this is not the proper place to post such things.