This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PMP21462: What are the benefits of using UCC28742 (High-Efficiency Flyback Controller With Optocoupler Feedback) in the implementation of a “magnetically resistant” power reference design?

Prodigy 720 points

Replies: 1

Views: 489

Part Number: PMP21462

What are the benefits of using UCC28742 (High-Efficiency Flyback Controller With Optocoupler Feedback) in the implementation of a “magnetically resistant” power reference design?

  • The PMP21462 is a 12-Watt, Magnetically Resistant, Quasi-Resonant Flyback Reference Design. It is designed for wide input (90-490 Vac input) and accounts for variance due to an external magnet. In order to make this reference design work robustly across a variety of conditions, a discontinuous conduction mode (DCM) is desirable. DCM allows for a simpler control loop that can work across wide input range.

    The Quasi-Resonant operation allows the controller to operate in DCM by utilizing valley-switching to reduce switching losses. The UCC28742 (High-Efficiency Flyback Controller With Optocoupler Feedback) was chosen because it offers this quasi-resonant switching capability to implement low cost output rectifiers.

    To learn more about the performance of this reference design under typical and stress test conditions, refer to section 2 "Testing and Results" of the User Guide for PMP21462.

    You can also download the design files (BOM, Schematic, Gerber) for this reference design from the PMP21462 folder.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.