This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PMP20859: What are the benefits of using TPS2372 (PoE High-Power PD Interface with Automatic MPS & Autoclass) in the implementation of a “smooth transition” PoE PD reference design?

Prodigy 720 points

Replies: 1

Views: 518

Part Number: PMP20859

What are the benefits of using TPS2372 (PoE High-Power PD Interface with Automatic MPS & Autoclass) in the implementation of a “smooth transition” PoE PD reference design?

  • The PMP20859 is a Dual-input redundant PoE PD reference design with the smooth transition feature. The smooth transition feature enables the delivery of non-interrupted output power. For the smooth transition to operate, the PoE inputs of the PD must stay connected to the Power Source Equipment (PSE). There is a maintain power signature (MPS) defined in the IEEE802.3bt PoE specification, which is a minimum load that must be maintained for a PSE to stay connected to a PD. The TPS2372 automatically detects when the minimum load is reached and applies a pulsed load (for reduced power dissipation) to satisfy the MPS.

    To learn more about the performance of this reference design under typical and stress test conditions, refer to section 2 "Testing and Results" of the User Guide for PMP208959.

    You can also download the design files (BOM, Schematic, Gerber) for this reference design from the PMP20859 folder.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.