This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PMP21513: What are the benefits of using UCC28742 and quasi-resonant flyback topology in the implementation of power supplies for audio applications?

Prodigy 720 points

Replies: 1

Views: 472

Part Number: PMP21513

What are the benefits of using UCC28742 and quasi-resonant flyback topology in the implementation of power supplies for audio applications?

  • PMP21513 is a fully tested TI Power Reference Design for 25/50-W audio applications. This design is able to run off a wide input voltage range of 85-265VAC.

    UCC28742 is a cost effective PWM controller used in this quasi-resonant (QR) flyback design. The QR switching operation of PMP21513 results in high efficiency across the range of loads required by audio systems (25 W continuous operation and 50 W peak). The transformer design allows for dual outputs and uses interleaved windings for more precise regulation of the 6 V output.

    UCC28742 provides constant-voltage using opto-coupled feedback, improving transient response to large load steps. Additional benefits include the ability to maintain low noise for sensitive audio signals (<2.5% of 24 V output).

    To learn more about the performance of this reference design under typical and stress test conditions, refer to section 2 "Testing and Results" of the User Guide for PMP21513.

    You can also download the design files (BOM, Schematic, Gerber) for this reference design from the PMP21513 folder.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.