Other Parts Discussed in Thread: ISO5852S, ISO5851
Hiii,
I am trying to implement the auto reset circuit (TIDA-00917, page no.11) in my gate driver. But when i analyzing the circuit i got a doubt. when RDY pin is low , the diode D10 becomes forward biased & C8 will discharge, this will cause a peak current to flow in the diode which is 5/0.2 = 25A , where 0.2ohm is approx diode forward resistance taken from diode datasheet. This current may destroy the device. Please solve my query.
Regards
Nagasahitya