This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01477: it is possible to add load cell to this board

Part Number: TIDA-01477
Other Parts Discussed in Thread: TIDA-00488

Dear Experts,

i have doubt in this board design, i have a idea to collect weight, humidity and temperature from multiple nodes, and one TIDA-01477 board is connect through UART with my GSM enabled board/ CC3220 wifi enable board for send the data's to server,

if this board design is suitable for my idea please suggest best load cell amplifier for this board,

how many node i can connect with this,

there is possible to get data's from particular node, because when my main board is send request to particular node, that node only must respond to main board.

how can i update the firmware through OTA to particular node.

if i powerup this board through 12v/10W solar panel, which converter or regulator is suitable for this.

 

thank you

  • TIDA-01477 is running TI 15.4-stack, which is a star-based protocol. TIDA-01477 operates as an end node, and it will communicate with a separate gateway that can be used to send out information to the cloud. This blog (e2e.ti.com/.../sensor-to-cloud) provides a brief overview to the protocol. For more specific questions about the TI 15.4-stack only, please open a new query and post to the Sub-1GHz forum (e.g., how many nodes, OTA firmware upgrade, etc).

    For solar panel, we have TIDA-00488. This shows how to use solar panel to power up an end node.