Other Parts Discussed in Thread: BQ76930, BQ34Z100-G1, TIDA-010030, BQSTUDIO
Hi,
I need to design an BMS which can charge 18s3p cells with the functions of reporting the state of charge and passive balancing. I really like the TIDA-00792 TI Reference Design. It almost fits what I need. But it can only handle up to 15 cells. Is it possible to add another chip to handle the extra 3 cells?
I also looked at the TIDA-01537 Design, which is scalable from 6s to 96s cells. But it seems to me that it doesn't report the SOC. Is that right? Is it possible to add that function?
Any advice would be greatly appreciated