Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
So I'm having a bit of trouble getting this IBIS model up and running in PSpice. I'm Using OrCad Capture.
Here is what I've done so far:
1. Open Model Editor
2. File > New
3. Model >IBIS Translator
4. Browse and select "am26lv32e.ibs" file. Note that as soon as I select it, the below files and folder are created:
am26lv32e.dml
am26lv32e.lib
am26lv32e_ibis2pspice.log
devices.dml
temp.lisp
signoise.run(Folder)
5. With Select ALL, Typ, and Use 2 V-t Tables selected I hit OK
6. 4 items appear in the Models List, 2 for the differential inputs, one labeled input that I assume is for the enable, and one labeled output.
7. Click File > ....
8. "Export to Part Library" is greyed out
Everything I've seen online uses "Export to Part Library" and I haven't found much for an alternative. If you have one that'd be great. If you know how to fix the model editor to work that would also be great. In every example I've seen in using "IBIS Translator" there was only one item in the Model List so I am not sure if there may be something special about this part or if perhaps I am improperly using Model Editor.
I opened Model Editor just by clicking "Edit PSpice Model" on another part then hitting "File > New" to clear out that parts IBIS info. I don't know if that would effect it but I'm used to being able to find Model Editor within the Cadence dropdown but the version my work owns seems to have things moved around a bit.