Other Parts Discussed in Thread: CSD19533KCS
Hello,
I would like to use the TIDA-01371 to have +55V @6A at the output, continuous service.
I am expecting high PSRR and Low Drop Voltage.
The circuit will be placed after an industrial SMPS with 200mVpp of ripple and I have to clean and isolate the output.
I would like to avoid the use of LCR filters.
I planned to add a heatsink at the CSD19533KCS.
Can I have the TINA file about the schematic reported at "TIDA-01371_E2_Positive-Regulator.SchDoc" pag 2 of 5?
So I can simulate the behaviours ... unfortunately I am not so skilled with TINA and I scare to introduce mistakes.
Regards.
Mario