Part Number: TIDA-00951
TIDA-00951 There are some questions about the design board.
The HV side FET is described as full bridge driven.
However, there is no working waveform for the FET when in charge mode.
Is it Phase Shift?
Or is it traditional Hard Switching?
And does the LV side FET operate with synchronous rectification?
Here is the Center tap question for Trans.
In the circuit diagram, it is connected to the center tap of Trans primary side and the capacitor center. What does it do?
Or what are the benefits?
Here are some questions about Boost Mode Working: Cold Start.
Can I remove the cold start circuit if the HV capacitor is always maintaining a voltage above 350V?
Thank you for your help.