This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

PMP20199: Required Parameter Changes in Schematic.

Prodigy 60 points

Replies: 2

Views: 94

Part Number: PMP20199

Hii Expert

The Design of PMP20199 has Output current as 560mA.I need a the current at output as 600mA.

Could you please suggest me that either the component/parameter to be changed or whatever the changes required  to obtain the current as 600mA.

Thankyou

With regards

D.Sravya

  • Hi D.Sravya,

    The design has some margin and will work at 0.6A.

    If you refer to section 6 in the test results, the current regulation is around ~0.63-4A.

    For additional margin, the only part that needs to change is the current sense resistor to a slightly lower value.

    Thanks,

    Robert

  • In reply to Robert Taylor1:

    Thank you

    Robert Taylor1

    It was helpful.

    With Regards

    D.Sravya.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.