Other Parts Discussed in Thread: UCC28C45
Good day.
i would like to ask if i could use this reference circuit with UCC28C45D?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gooi Wen,
There are two difference between the C42 and C45.
The C42 has wider hysteresis on the UVLO pin, this is very helpful in offline applications (AC input), using the C45 would mean making the bias capacitor much much larger.
The second difference is the duty cycle limit, C42 can go to 100% duty cycle which is helpful during startup, the C45 is limited to 50%.
So in general I would not recommend the switch.
Thanks,
Robert
Hi Gooi Wen,
No, we do not have any designs for AC/DC with the UCC28C45, it is not a good choice due to the limitations I listed above.
Thanks,
Robert