This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDA-00951: TIDA-00951 some components are not available

Intellectual 445 points

Replies: 7

Views: 314

Part Number: TIDA-00951

Hello,

i looked at the BOM files and i noticed that some of the components are not available for sale any more.

How can I replace them?

Best regards

Michael

  • Hi, Michael

    Could you show me those components not available, and the components your replacement.

    Dyson Guo

  • In reply to Desheng, Guo:

    Hi thank you for replying!

    i am a student that want to build that unit , and i am little bit lack of confident to choose substitute myself.

    thank you for the help.

                                Part Number                     Manufacturer     Description

     Obsolete         GRM188R70J105KA01D          MuRata        CAP, CERM, 1 µF, 6.3 V, +/- 10%, X7R, 0603            

      substitute       CL10B105KQ8NNNC                                   1µF ±10% 6.3V Ceramic Capacitor X7R 0603 (1608 Metric)

      link -       https://www.digikey.com/product-detail/en/samsung-electro-mechanics/CL10B105KQ8NNNC/1276-1024-2-ND/3886682

     

     

     Obsolete     GRM188R71E104KA01D       MuRata             CAP, CERM, 0.1 µF, 25 V, +/- 10%, X7R, 0603

     Substitute    GRM188R72A104KA35J        MuRata               0.1µF ±10% 100V Ceramic Capacitor X7R 0603 (1608 Metric)

       link      -             www.digikey.com/.../2612562

     

    Obsolete     GRM188R71H102KA01D   MuRata                CAP, CERM, 1000 pF, 50 V, +/- 10%, X7R, 0603

     Substitute       CL10B102KB8NNNC       Samsung            1000pF ±10% 50V Ceramic Capacitor X7R 0603 (1608 Metric)

    link      -            https://www.digikey.com/product-detail/en/samsung-electro-mechanics/CL10B102KB8NNNC/1276-1018-2-ND/3886676

     

     

    Obsolete        TK16E60W5,S1VX              Toshiba                          MOSFET, N-CH, 600 V, 915.6A, TO-220

    Substitute       STP28N65M2            STMicroelectronics                   MOSFET N-CH 650V 20A TO220

    link             www.digikey.com/.../5244932

     

     

    Another question - i am not sure what the xx is stand for - since i cannot find this part at  Coilcaft website i am asking that question.

    T3                  xx mH             FIS1xx           Coilcaft          Transformer, Current Sense              0.591 x 0.693 inch

    best regards

    Michael

     

  • In reply to michael coletti:

    Hi, Michael

    After looking through your list, only the MOSFET may have some effect to the efficiency, you can try that one.

    for the FIS1xx, it is an 50:1 current transformer. Please choose FIS105NL from PULSE. 

    Dyson Guo

  • In reply to Desheng, Guo:

    Hi thank you for the answer~!

    did you add a link or a serial number for new part or that you suggest that i will use the one that i mention?

    "       After looking through your list, only the MOSFET may have some effect to the efficiency, you can try that one.          "

     


    Best regards!

    Michael

  • In reply to Desheng, Guo:

    also there is an alternative for those transformers? i find it difficult to get them.

    T1 1   750343383R01 Wurth Elektronics TRANSFORMER, 4.5uH, 10%, THRU-8P
    T2 1   750343382R02 Wurth Elektronics TRANSFORMER, 45uH, THRU-20P
    T4 1 38uH 750343341 Wurth Elektronik Transformer, 50 uH, SMT

    as well as , is that component ok for use?

    https://www.digikey.com/product-detail/en/alpha-omega-semiconductor-inc/AOT10N60/785-1191-5-ND/2353856 

    note that the current is 10A and not 2A as mention in BOM.

    as a replacement for :

    Q10 1 600V AOT10N60 AOS MOSFET, N-CH, 600 V, 2 A, DPAK

    best regards,

    Michael

  • In reply to michael coletti:

    I think you already listed the substitutes as below

    Obsolete        TK16E60W5,S1VX              Toshiba                          MOSFET, N-CH, 600 V, 915.6A, TO-220

    Substitute       STP28N65M2

    Dyson Guo

  • In reply to michael coletti:

    Hi, 

    For those magnetics compoents, you may contact Wurth Elek for samples or datasheet. 

    and for the Q10, you could choose AOT10N60 as the BoM listed.

    Dyson Guo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.