This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDA-00288: TIDA-00288: Pins 33 and 32 on the TUSB8041 (EN_PORT3 & EN_PORT4) are not connected

Prodigy 20 points

Replies: 1

Views: 118

Part Number: TIDA-00288

Hello, we are currently in the process of incorporating the TIDA-00288 (TUSB8041) to a few different projects.

Looking at the TIDA-00288 reference schematics pins 33 and 32 on the TUSB8041 (EN_PORT3 & EN_PORT4) are not connected to anything. why is that?

pins 35 and 36 (EN_PORT1 & EN_PORT2) are connected to the TPS2003C, but why are pins 33 and 32 not connected to the two TPS2546?

Thanks,

Avi

  • Hi Avi,

    This is an older design and it looks like they wanted to showcase the battery charging capabilities of the TPS2546 devices on these ports including DCP charging.  DCP charging would be enabled when the upstream port is disconnected, under typical conditions the hub would disable the port power control in that case so instead they pulled the enables high to keep the TPS2546 devices on.

    Regards,

    JMMN

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.