This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01469: Issue regarding U4 IC

Prodigy 100 points

Replies: 1

Views: 94

Part Number: TIDA-01469

With reference to TIDA-10469,after insert battery in battery holder the voltage across C4 ,C10,C9,should be near to battery voltage i.e 3V and the Voltage across C18 should be 3.3V

So as per your design after giving 3V supply to the board i am getting voltage across C10 is 3V ,but across C9 is 1.6V and across C18 is 1.4V .On removing U4(TPS61291DRVR) I am getting voltage across C9 3.0V. so without U4, 3.0V i am getting across C9 

so please help me regarding this. 

1 Reply

  • Expert 8505 points

    Can you provide more detail on your system setup?

    • Do you have a Launchpad connected?
    • If powering from the battery, did you make sure to remove the jumper to disable the Launchpad's USB power supply and onboard emulator (e.g., remove all jumpers from P4 and P10)?
    • What is the voltage of LS_INT?


    If your question has been answered, please click  Verify Answer .

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.