Other Parts Discussed in Thread: LM5060
Hi,
My customer is looking into TIDA-01167 for a 24V battery truck application, but has the concerns below about the solution size and level of testing. Can you please comment and propose any changes or alternative solution if needed?:
I have read through the documentation for the reference design and it rises a few red flags to me. Why was it not tested up to the toughest spec (202V and 1 ohm) of ISO16750-2? I guess I know the reason, but omitting some graphs or tests makes me think that there is something less favourable. The fact that the LM5060 relies on 3 large external TVS’ to handle the peak voltage also affects the total footprint and BOM cost. Today we have one 200V 1.5kW SMC, one DPAK MOSFET, some discretes and it handles 250V steady state for about 30 seconds and passes the 202V 1R pulse 5 with Class A.
Thanks,
Antonio