Part Number: TIDA-00961
Hi,
I am running the system in open loop( INC_BUILD=1), new_ton_calc =20, and i am applying load of 333 ohms and input of 100V DC. In this build you are using only two switches. initially switching frequency is 1Mhzs and output voltage is 130V. But after sometime switching frequency is 200Khz and on period of active switch is very less (i.e around 6%) because of that stored energy is not enough to boost the voltage during this time whatever the input voltage we are giving that only coming across the load. Is this the reason after some time output voltage is 100V.
Thanks
yashwanth