Hello,
I recently installed TINA-TI 9.3.200.277 SF-TI on a Win10 pc.
Whenever I try to compile or ERC any of TINA's macros (the ones that come standard with the program) from its netlist viewer I get the following error:
Access violation at address 008B936B in module 'TINA.EXE'. Read of address 000004F9
Also when I try to ERC any schematic (even when it doesn't consist a macro) from the schematic editor I get the following error:
<InternalError|GraphGen.Init_Graph>
When I then press 'OK' I get the following message:
Access violation at address 0093001C in module 'TINA.EXE'. Read of address 00000408
And thirdly, when I try the steady state solver on any schematic I also get the <InternalError|GraphGen.Init_Graph> error.
Do any of you have an idea of what's causing this?
Any help would be greatly appreciated.
Regards,
Marius Bouwman