Part Number: TIDA-00951
Hello,
C12 | 1 | 0.1uF | ECW-F6104JL | Panasonic | CAP, CERM, 100 pF, 50 V, +/- 1%, C0G/NP0, 0603 |
at the BOM file the part number is ECW-F6104JL, but this part number take me to 630V capacitor
which one is the correct one the 50v or the 630?
the same part number is mention in c8 as well
C8 | 1 | 0.1uF | ECW-F6104JL | Panasonic | CAP, Film, 0.1 µF, 1000 V, +/- 10%, TH |
which one is the correct one the1000v or the 630?
Thank you very much
Michael