This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01494: U7 (UCC24612), ISO_12V question

Part Number: TIDA-01494
Other Parts Discussed in Thread: UCC24612, TIDA-010015, UCC256301

Hi Sir,

In EVM for http://www.ti.com/lit/ug/tidudf3/tidudf3.pdf

There is ISO_12V at U7(UCC24612), i.e. external input voltage, can it obtain from EVM output 24V by linear regulator?

Or it must need to add one more PWM IC and transformer to provide this 12V

Regards,

Driscoll