Part Number: TIDA-00527
Other Parts Discussed in Thread: TIDA-010035, THVD2450
Hello,
I read the reference design TIDA-00527 (RS-485 Power Over Bus Reference Design) and TIDA-010035 (Power Line Communication Using RS-485 Simulation).
The solution is simple and useful.
But I have the maain question and secodnary question.
--> Main question: how many current I can draw without signal degradation? Some datas: 30V applied as DC component to RS485. Speed 9600bps (o 19.200bps). Distance: not more of 200m. Can I power my slave node that has a current consumption of 200mA? It's clear the inductor must can support not less of 500mA and the copper section of cable must be enought to avoid too much drop voltage.
--> Secondary question: the maximum voltage appliced to RS485 ad DC component is maximum 36V. Which transceiver You suggest (powered at 3,3V).
Thank You and Best Regards
Federico Battaglin