Other Parts Discussed in Thread: UCD3138128
Hello,
I'm working on a project that has similar specs to the TIDA-00653 for an automotive application. I just had a few questions about the design:
1. My output voltage is in the range of 11.5 V to 14.5 V, 14 V nominal. To meet this spec, I figured I would change the feedback resistor values, as well as use higher voltage rating capacitors at the output. Would TI recommend any additional changes?
2. Does the UCD3138128 support CAN? I could not find any information in the datasheet but I noticed the CAN transceiver in the schematic.
Thanks,
Tharindu