This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01352: TIDA-01352 question

Part Number: TIDA-01352
Other Parts Discussed in Thread: LM5030, DAC60004

Hi all,

We are promoting TIDA-01352, customer has following questions:

1. Why TIDA use non-isolation feedback while there is an isolation feedback on LM5030 datasheet? Do customer need isolation feedback or not?

2. What is the use of VoutC and VoutD of DAC60004? Can customer use one DAC60004?

  • Hello Jeff,

    Please find answers below:

    1. The isolation feedback depends on the customer's application. For TIDA-01352, the input was assumed to be coming from AC/DC board (with inbuilt isolation). That is why isolation is not included in TIDA-01352 schematic. However, if isolated feedback is required for LM5030, it can be added as highlighted in the datasheet of LM5030.

    2. VoutC & VoutD are extra outputs which can be used by customers for any other control requirements. Yes, customer can use one DAC60004 to control all 4 outputs.

    Regards,

    Sanjay R. Pithadia