Hi Team,
I would like to use the following Potetiometeron TINA-TI.
But I don't understand how to use it if I control the resistance of the potentiometer by voltage. (I mean how to set the properties.)
This is that properties.
- The resistance is for Max resistance value.
- The setting is the resistance position of this potentiometer.
And how should we set any other parameter if we want use the following condition?
Resistance range : 0 ~ 10k
Voltage range (by VG1): 0~ 10V. (Max voltage is 10V)
Best Regards,
Koji Hamamoto