Hello!
The nominal dc-bus voltage of the TIDA-00779 is chosen 390 V, which is controlled by a PFC circuit. I know that this value is considered as VDC>Vin_max*sqrt(2), as VDC>270*sqrt(2).
I, however, think this voltage value for dc bus is so high to drive a 220 V three-phase motor. So, the input voltage range should be reduced which is not acceptable for such practical device.
Can anyone explain it for me?
HE