This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: TIDA-010054

Part Number: TIDA-010054

Helo

I design DAB bidirectional conveter with Input voltage 400V, Output voltage 44-58V, Output power 3KW, switching frequency 200Khz. If I will not use peak current mode control and I will use only average voltage mode control for both power transfer energy, is necessary only one Capacitor in series with transformer which avoid saturation of transformer? In  TIDA-010054 is only one this capacitor on the High voltage side, which is not use finally.

Thank you