Part Number: PMP4334
Hi,
regarding the schematics for the PMP4334, I've noticed that Q1, ZD4, R17 are not assembled in the CBA. My question comes regarding how much would I need these components if I have dimming implemented for the LEDs. On the datasheet from the UCC28810D they recommend the usage of such a circuitry... If I add those components would it work as is or would I have to re-rout some parts of the circuitry (other than remove the by-pass 0 ohm R39) ?
Another question regarding the Output of the Transformer T1. The pin 9 is outputting 12V (+12VS). Why does it also have VAUX in the same line, isn't it also 12V and why was Q9 removed from that line?
Sorry for asking so many questions!
Your support would be highly appreciated!
Best regards,