CCS/TIDA-00121: Battery charging current Limitation Problem

Prodigy 40 points

Replies: 3

Views: 32

Part Number: TIDA-00121

Tool/software: Code Composer Studio

Hi Experts,

Thanks ti to the design of TIDA-00121.I usied the design for  12W,30w,45W,60W and 75W light by changing the firmware as per the requirement and the results are good.

When it come to battery charging using solar panel, was not able to limit the charging current by changing the values to the variable i.e. CC_LIMIT.

So if we need to limit charging current at 6A if the panel sourcing current is 5 A Design working OK or If we change the wattage of panel i.e. sourcing current Max 20A then it is not controlling charging current.

Any Help on this issue thank in advance.

Thanks & Regards

A Hari Krishna

3 Replies